topleft
SKF Online Catalog
Online Catalog

Press office

September 2, 2008
SKF acquires Italian company to strengthen its vehicle aftermarket business 
SKF has signed an agreement to acquire GLO s.r.I and its manufacturing operation in Italy...

September 1, 2008
SKF, your one-stop source for Asian kits 
Look no further with SKF Asian kits! Today, Asian vehicles represent 20% of the total car parc in Europe with an 8-10% annual growth rate. With this in mind, SKF has invested time and resources in extending the Asian product range to meet all its customer needs and improving availability by taking advantage of its global production facilities and development centre in Singapore.

July 31, 2008
SKF at Automechanika, Franfurt 2008! 
SKF is pleased to announce its presence to the 2008 edition of Automechanika, the leading international trade fair for the automotive aftermarket industry...

April 15, 2008
SKF launches its electronic catalog on CD 
SKF has launched its electronic catalogue on CD including all its Automotive vehicle product lines

April 1, 2008
SKF elected AD International Supplier of the Year 2007 
For the second time in 4 years, SKF has received the ADI Supplier of the Year award for 2007.

March 1, 2008
Latest CV-joint technology in SKF drive shaft range (VKJ) for RENAULT Megane and Grand Scenic  
SKF has extended the drive shaft range with the latest CV-joint technology based on an eight ball design that reduces the weight and the volume of the transmission, striving for reduced fuel consumption.

February 15, 2008
SKF launches a new V-belt and Multi-V belt range to complete its auxiliary drive offer 
When the auxiliary belt needs replacement, it often implies that the belt tensioner or idler pulley are worn. SKF strongly recommends to replace the whole system, i.e the belt as well as the tensioner or idler pulley and offers the most complete auxiliary kit range of the market.

February 1, 2008
SKF equip the “Car of the year 2008” - Fiat 500 
SKF supplies the popular Fiat 500 , elected as “Car of the year 2008”, with front and rear axle wheel bearings, constant velocity joints as well as engine products for the timing system, the auxiliary drive and the cooling system.

January 15, 2008
SKF Universal boots for optimized repair time  
The new SKF universal boot kit – VKJP 01000 - is now available on the market. Its geometry and material are especially designed to be mounted on all types of passenger cars. The compound of the boot is a special mix of rubber - making it easy to mount and shape around the joint without having to remove the shaft.



Search

UK Flag